AXIS#.VL.THRESH
Description
AXIS#.VL.THRESH sets the user overspeed fault threshold. This threshold becomes the overall overspeed fault threshold (AXIS#.VL.VFTHRESH) if it is less than the motor speed threshold (1.2 x AXIS#.MOTOR.VMAX), and for AXIS#.MOTOR.TYPE = 6 if it is less than the motor back EMF overspeed threshold ((1.02 x 1000 x VBUS.OVFTHRESH) / (AXIS#.MOTOR.KE x sqrt(2))).
The value is considered an absolute value, hence it applies for both negative and positive velocities.
Example
AXIS#.VL.THRESH is set to 600 rpm. A velocity (AXIS#.VL.FB ) of 700 rpm will generate an over speed fault.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Rotary: RPM See Velocity Units for details. |
Range |
Depends on units. See Velocity Range for details. |
Default Value |
3,600 RPM Depends on units. See Velocity Units for details. |
Data Type |
Float |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO![]() |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.VL.THRESH | 0x5011 | 0x8 | UDINT | - | Velocity | RW | False |
AXIS2.VL.THRESH | 0x5111 | 0x8 | UDINT | - | Velocity | RW | False |